AXIS#.IL.COGCOMP.TEACH.STATUS
Description
The status of the Cogging Compensation teach phase.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 - Cogging compensation in not running. 1 - Cogging compensation teaching algorithm is running 2 - Cogging compensation table has been successfully created 100 - Cogging compensation encountered an error while teaching |
| Default Value | 0 |
|
Data Type |
U8 |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL |
0x500A | 0x22 | USINT | 1:1 | - | RW | False |
| AXIS2.IL.COGCOMP.TEACH.STATUS | 0x510A | 0x22 | USINT | 1:1 | - | RW | False |